• AVR Freaks

Hot!CLC Ouput as UART input

Author
werner
Starting Member
  • Total Posts : 66
  • Reward points : 0
  • Joined: 2003/11/07 12:38:58
  • Status: offline
2019/07/04 12:04:08 (permalink)
0

CLC Ouput as UART input

Hi,
I am using PIC18F27K42 with has feature CLC. Is it possible, to route the output of one CLC cell to uart rx ?
In datasheet block diagramm is an arrow from output to peripherals, but no more info.
 
Thanks
Werner
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5