• AVR Freaks

Reset HLT Timer Postscaler?

Author
acharnley
Super Member
  • Total Posts : 563
  • Reward points : 0
  • Joined: 2016/05/01 06:51:28
  • Location: 0
  • Status: offline
2019/07/04 02:31:35 (permalink)
0

Reset HLT Timer Postscaler?

Hi,

Is it possible, does it occur behind the scenes when you write to TMR2 = 0 etc?

The reason I ask is on the PIC16F1788 the CLC's use the postscale value. If I've reset the TMR manually then it'll still be incorrect.

Andrew
#1

1 Reply Related Threads

    coffee critic
    Super Member
    • Total Posts : 392
    • Reward points : 0
    • Status: offline
    Re: Reset HLT Timer Postscaler? 2019/07/11 16:49:46 (permalink)
    0
    I think the part number is incorrect.  The 1788 does not have CLC. 

    n_*$
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5