• AVR Freaks

Hot!RN4871 - how to control the GPIO pin as output?

Author
teslabox
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2013/07/18 03:20:00
  • Location: 0
  • Status: offline
2019/07/01 06:22:02 (permalink)
0

RN4871 - how to control the GPIO pin as output?

Hi guys,
 
How to control the GPIO pin as output of RN4871 module from my smartphone? I would like to control one MOSFET or relay via Bluetooth withou using any additional micocontroller. Is there any simple example how to do it? Is it possible in Transparent UART mode? Or in other mode?
I cannot find any helpful examples in Microchip area in the Internet.
 
I will be gratefull for help :).
 
Best regards,
Jacob
 
 
post edited by teslabox - 2019/07/01 06:29:31
#1

0 Replies Related Threads

    Jump to:
    © 2019 APG vNext Commercial Version 4.5