• AVR Freaks

Hot!Harmony 3 Framework downloader freezes after download Packages

Author
asvoria
New Member
  • Total Posts : 11
  • Reward points : 0
  • Joined: 2018/11/02 05:11:20
  • Location: 0
  • Status: offline
2019/06/26 19:02:36 (permalink)
0

Harmony 3 Framework downloader freezes after download Packages

Hi,
I just started to install MPLAB, and trying to setup the environment to work with Harmony 3.
When I started the Harmony 3 framework downloader, following the steps, 
after step: 4. Download Packages, the instruction ask me to click next, but the next button didn't work.
I'm unable to move to step 5. Package Configuration. Can't cancel, can't do anything but have to end the whole MPLAB.
Any idea what to do?
 Using MPLAB X IDE v5.20
post edited by asvoria - 2019/06/26 19:07:02
#1

1 Reply Related Threads

    TS9
    Super Member
    • Total Posts : 791
    • Reward points : 0
    • Joined: 2010/05/07 10:52:22
    • Status: offline
    Re: Harmony 3 Framework downloader freezes after download Packages 2019/06/27 00:42:15 (permalink)
    0
    Hi,
     
    I have installed Harmony 3 framework MPLAB X 5.20 without any issue ?
     
    What is the RAM Size in your System ?
    What is the type of Hard disk , SSD or HDD ?
     
    Can you check with other system (PC) ? May be other Hardware Issue .
     
    --
    TS9
     
    #2
    Jump to:
    © 2019 APG vNext Commercial Version 4.5