• AVR Freaks

Helpful ReplyHot!Reverse Engineering PM3 RS232

Author
masterpic
New Member
  • Total Posts : 6
  • Reward points : 0
  • Joined: 2016/03/18 13:22:34
  • Location: 0
  • Status: offline
2019/06/25 17:04:05 (permalink)
0

Reverse Engineering PM3 RS232

I want to link my PM3 to database for serializing devices. I think the easiest way to communicate to pm3 will be rs232.
 
Anyone know the format of image? I am thinking to use a device in between the pm3 and PC with ipe to read and pass along communications. I was just wondering if anyone has already figured this out.
 
I found some hints here:
https://www.microchip.com/forums/m119930.aspx
#1
zdenekjs
Super Member
  • Total Posts : 197
  • Reward points : 0
  • Joined: 2013/02/13 23:04:26
  • Location: 0
  • Status: offline
Re: Reverse Engineering PM3 RS232 2019/06/25 19:56:33 (permalink) ☄ Helpfulby masterpic 2019/06/26 08:42:23
0
Why use a PM3 where you have to reverse engineer it?  I used a softlog ICP2 for programming:
http://softlog.com/index.asp?page=ICP2%28G3%29&parentid=2
They have a DLL to control it.  At least then you'd have a documented, supported interface.
 
Who knows what microchip will change down the road?  I'd be afraid that plugging the PM3 into a computer with a newer version of MPLAB would break things.  It did for me with PK3CMD, and that was just from the command line.  Some firmware update did something wierd, so I had to load the older MPLAB and reprogram my PICkit3.
 
Disclosure: I have no association with them other than as a happy user.
 
#2
Sudheer Herle
Super Member
  • Total Posts : 415
  • Reward points : 0
  • Joined: 2012/03/30 05:41:29
  • Location: Bangalore ,India
  • Status: offline
Re: Reverse Engineering PM3 RS232 2019/06/25 20:28:42 (permalink)
5 (1)
Serializing devices? Please elaborate.
Microchip offers ipecmd and also SQTP feature. Please refer those.
#3
Jump to:
© 2019 APG vNext Commercial Version 4.5