• AVR Freaks

Hot!PIC32MZ harmony Tutorial

Author
Mohammed_Hassan
Starting Member
  • Total Posts : 31
  • Reward points : 0
  • Joined: 2019/03/13 06:05:20
  • Location: 0
  • Status: offline
2019/06/25 07:02:00 (permalink)
0

PIC32MZ harmony Tutorial

Hello guyz, 
I am working in a project with PIC32MZ0512EFF064 controller and need to make a prototype up and running in 2 weeks.
the decision has been made to use Harmony v2.6. 
 
IS there any tutorial for using Harmony for configuring PIC32MZ controllers? 
I searched a lot and could not find any helpful links.
 
Thanks in advance for the support.
 
#1

5 Replies Related Threads

    Jim Nickerson
    User 452
    • Total Posts : 6259
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: offline
    Re: PIC32MZ harmony Tutorial 2019/06/25 07:22:48 (permalink)
    0
    This is a very short amount of time.
    Copy one of the Microchip development kits and use one of the Harmony demos.
    #2
    Mohammed_Hassan
    Starting Member
    • Total Posts : 31
    • Reward points : 0
    • Joined: 2019/03/13 06:05:20
    • Location: 0
    • Status: offline
    Re: PIC32MZ harmony Tutorial 2019/06/25 07:34:39 (permalink)
    0
    JANickerson
    This is a very short amount of time.
    Copy one of the Microchip development kits and use one of the Harmony demos.


    Could you help me by suggestions? 
    mainly I need to use ADC, DMA, I2C, GPIO,PWM and UART peripherals and for sure configure clock and timers.
     
    Thanks for your help in advance.
    #3
    NKurzman
    A Guy on the Net
    • Total Posts : 17846
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: online
    Re: PIC32MZ harmony Tutorial 2019/06/25 07:42:53 (permalink)
    0
    https://www.microchip.com/mplab/mplab-harmony
     
    Click on the Training getting Started Tab.
     
    There are also two books availabler for Harmony, But Note Harmony is a Moving Target. It is Posible that they are out of date.
    #4
    LostInSpace
    Super Member
    • Total Posts : 265
    • Reward points : 0
    • Joined: 2016/03/11 22:47:59
    • Location: 0
    • Status: offline
    Re: PIC32MZ harmony Tutorial 2019/06/25 21:14:18 (permalink)
    0
    There are many resources on getting started in Harmony.
     
    Two written tutorials,
    http://ww1.microchip.com/downloads/en/DeviceDoc/MPLAB%20Harmony%20Tutorial%20-%20Creating%20Your%20First%20Project.pdf
    http://ww1.microchip.com/downloads/en/DeviceDoc/90003177A.pdf
     
     
    The Microchip Youtube Channel on Harmony,
    https://www.youtube.com/watch?v=wyUPpTfxRDE&list=PL9B4edd-p2agL42JeLytmJrRNh6CsyGiS
     
    At the bottom of the product page, under documentation you will see a heading called,
    "Code Examples" - There is useful information there.
     
    And as mentioned - Harmony has a lot of example projects to look at, one for nearly every peripheral. I suggest that you spring for one of the PIC32 Development boards (they are cheap) so that you can get the examples running very quickly.
     
    Hope this helps  :-)
     
     
     
    #5
    LostInSpace
    Super Member
    • Total Posts : 265
    • Reward points : 0
    • Joined: 2016/03/11 22:47:59
    • Location: 0
    • Status: offline
    Re: PIC32MZ harmony Tutorial 2019/06/25 21:24:06 (permalink)
    0
    Also - In the future, for 'Harmony' related posts use this forum, your questions may get answered quicker,
    https://www.microchip.com/forums/f291.aspx
     
    #6
    Jump to:
    © 2019 APG vNext Commercial Version 4.5