• AVR Freaks

Hot!Have anyone had success in hid over gatt with rn4871?

Author
JoniS
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2019/06/24 07:13:14
  • Location: 0
  • Status: offline
2019/06/24 20:57:04 (permalink)
0

Have anyone had success in hid over gatt with rn4871?

I have found on old thread with some code(https://www.microchip.com...aspx?m=977216&p=1) but sadly it's code without any explaining.

I'm particularry wondering the shw commands, if i understand something those are used to update the charasterics.

Ie. SHW,(PnPID),013A5B2A6B8C90

Am I supposed to run LS command and get handle so it would be "SHW, (handle), xxxxxxx"

And which charasterics is the one I should update to send key events? Will transparent uart service work simultaneously with hid over gatt?
#1

1 Reply Related Threads

    JoniS
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2019/06/24 07:13:14
    • Location: 0
    • Status: offline
    Re: Have anyone had success in hid over gatt with rn4871? 2019/06/30 02:42:31 (permalink)
    0
    I can answer to myself partly now, i got my android device to identify the RN4871 as "Input device", well after soft bricking it X times.
     
    Well, cant get any input to my phone thought. i guess its because the module does not like self defined "device information service" and loses it on reboot so one cant access the handle's of charasterics anymore -.- i guess this is the dead end everyone else who attempted this did come across too, atleast based on my search.
     
    Time to buy another module i guess.
    #2
    Jump to:
    © 2019 APG vNext Commercial Version 4.5