• AVR Freaks

Hot!Compiler Question

Author
mikenycz_aao
New Member
  • Total Posts : 9
  • Reward points : 0
  • Joined: 2018/09/27 11:07:22
  • Location: 0
  • Status: offline
2019/06/24 06:32:27 (permalink)
0

Compiler Question

I have been using MPXLAB with the XC16 compiler installed. I am now looking at a device that would require the XC8 compiler. Is it OK to have both compilers installed at the same time? Or do I need to have a separate installation of MPXLAB for each compiler that I want to use?
 
Thank you,
Mike Nycz
#1

2 Replies Related Threads

    ric
    Super Member
    • Total Posts : 26968
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: offline
    Re: Compiler Question 2019/06/24 06:37:05 (permalink)
    +1 (1)
    You can have both installed, no problem.
    You can even have multiple versions of the same compiler installed, and MPLABX will remember for each project which version should be used.
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    GeorgePauley
    Moderator
    • Total Posts : 1239
    • Reward points : 0
    • Joined: 2009/12/01 13:59:30
    • Location: Chandler AZ
    • Status: offline
    Re: Compiler Question 2019/06/24 14:19:07 (permalink)
    +2 (2)
    And you can install multiple versions of both MPLAB X and XC* too!
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5