• AVR Freaks

Hot!Harmony V3 - where is the PMP

Author
Chris_Bell
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2019/06/17 23:16:35
  • Location: 0
  • Status: offline
2019/06/23 12:02:23 (permalink)
0

Harmony V3 - where is the PMP

I have recently installed MPLABX V5.30 with XC32 V2.20 and downloaded the following repo's using the Harmony 3 Framework Downloader:
csp V3.3.0, core V3.3.0, bsp V3.3.0, mhc V3.3.0, dev_packs V3.3.0, crypto V3.2.2 and net V3.3.0

Our current design which is being migrated to the PIC32MZ2048EFM144 device utilises the pmp to interface with an FPGA. However I cannot find
the pmp peripheral in the available components within the Harmony 3 Configurator.

Does anyone know where I can find the files for this peripheral.

Many thanks.


#1

3 Replies Related Threads

    tixmcprods
    New Member
    • Total Posts : 12
    • Reward points : 0
    • Joined: 2019/06/12 15:33:51
    • Location: 0
    • Status: offline
    Re: Harmony V3 - where is the PMP 2019/06/25 23:08:31 (permalink)
    0
    Hello,
    Already asked for this to support, no support for MX nor MZ at the moment, because of beta release.
    Coming second half 2019...
    Waiting for this too :)
    Best regards.
    #2
    Chris_Bell
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2019/06/17 23:16:35
    • Location: 0
    • Status: offline
    Re: Harmony V3 - where is the PMP 2019/06/25 23:14:36 (permalink)
    0
    Thanks for the reply.
    #3
    tixmcprods
    New Member
    • Total Posts : 12
    • Reward points : 0
    • Joined: 2019/06/12 15:33:51
    • Location: 0
    • Status: offline
    Re: Harmony V3 - where is the PMP 2019/08/01 04:13:45 (permalink)
    0
    Hello,
    A new update is out and now PIC32MX and MZ are not in "Beta release" anyway !
    Have to test it in some days and check if other libraries are missing.
    Stay in contact.
    Best regards.
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5