Re: Bug Found on MCCs IOC configuration, PIC16F1574
2019/11/06 03:27:37
(permalink)
Hi, PA91
I appreciate that you are reweing older messages in this forum,
to confirm that reported problems have been corrected in the latest release of
PIC10/PIC12/PIC16/PIC18 library v1.78.0
The original message was written long before the v1.78.0 was released.
Wording of the reply, however seem to imply that the original poster should rather have used a version of the library that was not yet released, and thus the reply appear as arrogant.
Please acknowledge the reported problem as real at the time it was reported,
before stating that your test indicate that the issue have been corrected in the latest release.
Also, please be aware that there seem to be something wrong with the Microchip website download service.
Trying to download PIC10/PIC12/PIC16/PIC18 library v1.78.0 ,
is causing a big page of gibberish text to appear, not a file to be downloaded.
Same problem whether trying to download from MCC webpage, or from within MPLAB X Notifications window.
This is with Firefox running on a PC with Windows 7.
So v1.78.0 isn't available to me.
Mysil