• AVR Freaks

Helpful ReplyHot!PC IP extraction

Author
PS225
New Member
  • Total Posts : 13
  • Reward points : 0
  • Joined: 2018/08/26 22:39:53
  • Location: 0
  • Status: offline
2019/06/22 02:27:05 (permalink)
0

PC IP extraction

Hello!
I am using PIC32 ESK II(with MPLAX X IDE v5.15) and trying to do some learning on networking side. I need to extract PC ip address and MAC address using some APIs(if any). Is there some method to implement it??
Sorry if its a stupid question, but i am a beginner here and any help would be much appreciated.
 
Thanks.
#1
crosland
Super Member
  • Total Posts : 1584
  • Reward points : 0
  • Joined: 2005/05/10 10:55:05
  • Location: Bucks, UK
  • Status: offline
Re: PC IP extraction 2019/06/22 07:50:19 (permalink)
4 (1)
This is a PIC forum. I would ask on Stack Overflow.
#2
PS225
New Member
  • Total Posts : 13
  • Reward points : 0
  • Joined: 2018/08/26 22:39:53
  • Location: 0
  • Status: offline
Re: PC IP extraction 2019/06/23 21:32:51 (permalink)
0
But here i am trying to get the PC ip and mac address through programming.
#3
rainad
Super Member
  • Total Posts : 1192
  • Reward points : 0
  • Joined: 2009/05/01 13:39:25
  • Location: 0
  • Status: offline
Re: PC IP extraction 2019/06/24 07:08:27 (permalink) ☄ Helpfulby PS225 2019/06/25 22:23:17
5 (1)
You can open a server on the PIC32 side and you connect to it from the PC, you can ask for the TCP_SOCKET_INFO. That will give you the remote party IP address.
For the MAC, then make an arp query: either from the command line in he console or through the ARP API in your program.
 
#4
PS225
New Member
  • Total Posts : 13
  • Reward points : 0
  • Joined: 2018/08/26 22:39:53
  • Location: 0
  • Status: offline
Re: PC IP extraction 2019/06/25 22:25:29 (permalink)
0
Thank you :)
#5
Jump to:
© 2019 APG vNext Commercial Version 4.5