• AVR Freaks

Hot!How to Program ATtiny1616 for SPI Interface as a Slave Device.

Author
embeddedshiv
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2018/03/29 06:03:01
  • Location: 0
  • Status: offline
2019/06/21 06:25:21 (permalink)
0

How to Program ATtiny1616 for SPI Interface as a Slave Device.

Hello Community,
 
I am working on ATtiny 1616 8 bit microcontroller with atmel studio development tool.
For configuring the ATtiny I am using atmel start configurations.
 
But I don't think that It (Atmel Start) supports all possible setups. 
For Ex.
1. I am not able to find the Interrupts settings for the Receive Complete Interrupt, Slave Select Trigger Interrupt etc... 
 
will you please help me to configure a ATtiny1616 SPI interface as a Slave device?...
 
Regards,
Shiv Patil.
#1

1 Reply Related Threads

    ric
    Super Member
    • Total Posts : 25562
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: How to Program ATtiny1616 for SPI Interface as a Slave Device. 2019/06/21 16:01:19 (permalink)
    0
    You're mainly talking to PIC people here.
    All the Atmel folk can still be found at https://community.atmel.com/
     
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5