• AVR Freaks

Hot!USB3320, external REFCLK and suspend / resume

Author
timistof
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2019/04/11 14:27:14
  • Location: 0
  • Status: offline
2019/06/20 14:32:06 (permalink)
0

USB3320, external REFCLK and suspend / resume

I'm using an external oscillator to supply REFCLK to the USB3320 in a bus powered usb device. To support peripheral suspend / resume, the MCU connected to the USB3320 has to disable this clock in order to meet the maximum 2.5 mA usb suspend current, since the oscillator uses about 4 mA when kept running.
Maybe I'm missing something from the datasheet, but how exactly is the PHY supposed to notify the MCU about a resume command if REFCLK is stopped? Doesn't it need it for that?
Or does the resume current limitation imply that an external oscillator is off the menu and I should just use the XO instead?
post edited by timistof - 2019/06/20 16:02:21
#1

1 Reply Related Threads

    timistof
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2019/04/11 14:27:14
    • Location: 0
    • Status: offline
    Re: USB3320, external REFCLK and suspend / resume 2019/06/24 15:11:40 (permalink)
    0
    After a more thorough inspection of the ULPI protocol, I found that in low power mode, the usb linestate is reflected on the ULPI databus. When the host issues a resume and a linestate change / interrupt occurs on the UPLI bus, the MCU sees this, re-enables refclk, wakes up the PHY and resumes operation.
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5