• AVR Freaks

AnsweredHot!Stopwatch tool does not take into account frequency settings of Simulator

Author
yildizabdullah
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2019/01/02 02:41:35
  • Location: 0
  • Status: offline
2019/06/20 03:46:07 (permalink)
0

Stopwatch tool does not take into account frequency settings of Simulator

Regardless of the changes in frequency of the simulator, I always see the same output in Stopwatch window when debugging my project.
 
I use MPLAB X IDE v5.10. Is there something wrong with Stopwatch or am I missing something?
#1
domble
Senior Member
  • Total Posts : 120
  • Reward points : 0
  • Joined: 2007/01/25 04:11:53
  • Location: 0
  • Status: offline
Re: Stopwatch tool does not take into account frequency settings of Simulator 2019/06/20 06:35:15 (permalink) ☼ Best Answerby yildizabdullah 2019/06/20 06:50:49
+2 (2)
Try closing and re-opening mplabx.  Seems to be a new feature for 5.10, same with ICD3/PICkit3 target power on/off switching (and at a guess, multiple other project settings).  Used to work for older versions.
 
dom.
 
#2
GeorgePauley
Moderator
  • Total Posts : 1123
  • Reward points : 0
  • Joined: 2009/12/01 13:59:30
  • Location: Chandler AZ
  • Status: offline
Re: Stopwatch tool does not take into account frequency settings of Simulator 2019/06/20 10:46:06 (permalink) ☄ Helpfulby yildizabdullah 2019/06/20 11:29:09
+4 (4)
I can confirm that restarting MPLAB X applies the new simulator settings in the stopwatch window.  It looks like stopwatch reads the scale once at startup and then never again.
#3
1and0
Access is Denied
  • Total Posts : 9291
  • Reward points : 0
  • Joined: 2007/05/06 12:03:20
  • Location: Harry's Gray Matter
  • Status: offline
Re: Stopwatch tool does not take into account frequency settings of Simulator 2019/06/20 12:51:31 (permalink)
+1 (1)
GeorgePauley
I can confirm that restarting MPLAB X applies the new simulator settings in the stopwatch window.  It looks like stopwatch reads the scale once at startup and then never again.

Can we expect this to change any time soon?  Or is it going to be a "feature" of MPLAB X?
 
#4
Jump to:
© 2019 APG vNext Commercial Version 4.5