• AVR Freaks

Hot!Harmony v3 - No MCU's to select

Author
dmccric
Senior Member
  • Total Posts : 159
  • Reward points : 0
  • Joined: 2006/05/30 08:13:15
  • Location: Bradford, England
  • Status: offline
2019/06/18 08:24:22 (permalink)
0

Harmony v3 - No MCU's to select

I have installed the latest versions of MPLAB X v5.20 and Harmony v3 but when I create my project it will not allow me to finish creating the project as there is no list of processors to choose from.
 
I have rebooted, re-installed, etc. Has anyone had the same problem?
 
Regards
#1

10 Replies Related Threads

    Jim Nickerson
    User 452
    • Total Posts : 6736
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: offline
    Jim Nickerson
    User 452
    • Total Posts : 6736
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: offline
    Re: Harmony v3 - No MCU's to select 2019/06/18 08:33:58 (permalink)
    0
    I see you have version 3, maybe this is of more help https://github.com/Microc...Harmony.github.io/wiki
    #3
    dmccric
    Senior Member
    • Total Posts : 159
    • Reward points : 0
    • Joined: 2006/05/30 08:13:15
    • Location: Bradford, England
    • Status: offline
    Re: Harmony v3 - No MCU's to select 2019/06/18 14:24:00 (permalink)
    0
    I have looked at both of these tutorials and none have helped me. Still the same issue, I have installed this on both my laptops and both have the same issue. I cannot see any target devices to select.
    #4
    dmccric
    Senior Member
    • Total Posts : 159
    • Reward points : 0
    • Joined: 2006/05/30 08:13:15
    • Location: Bradford, England
    • Status: offline
    Re: Harmony v3 - No MCU's to select 2019/06/19 00:57:28 (permalink)
    0
    I have now managed to create a project by adding the target MCU in manually, PIC32MX795F512L.
    I then selected the Configurator from the tools menu and I now get another error.
    See attached image.
     
    Any ideas?
     
     

    Attached Image(s)

    #5
    Jim Nickerson
    User 452
    • Total Posts : 6736
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: offline
    Re: Harmony v3 - No MCU's to select 2019/06/19 07:13:30 (permalink)
    0
    I have not used Harmony v3 for any Pic32Mx devices, only v2
    #6
    paulmtcuk
    Junior Member
    • Total Posts : 52
    • Reward points : 0
    • Joined: 2007/08/23 05:16:51
    • Location: 0
    • Status: offline
    Re: Harmony v3 - No MCU's to select 2019/06/19 08:47:09 (permalink)
    0
    I wouldn't add manually. 
     
    did you follow the steps in https://www.microchip.com/forums/m1101397.aspx ?
     
    When you create a new Harmony v3 project you must click on "Launch Framework Downloader" to download the latest framework from github. Did you do this?  You can redownload to refresh -- You must select at least some core packages from the catalog by checking the download tick box and click "Download" before "Next". After which the framework path must match that of the downloaded files and all supported PICs at the time of your download will be shown after "Next >" in to Project settings step. 
     
    post edited by paulmtcuk - 2019/06/19 08:49:19
    #7
    paulmtcuk
    Junior Member
    • Total Posts : 52
    • Reward points : 0
    • Joined: 2007/08/23 05:16:51
    • Location: 0
    • Status: offline
    Re: Harmony v3 - No MCU's to select 2019/06/19 08:51:20 (permalink)
    0
    (Couldn't edit)
     
    Did you follow https://github.com/Microchip-MPLAB-Harmony/mhc/wiki
     
    At which step did you get to?
    #8
    EngSam
    New Member
    • Total Posts : 18
    • Reward points : 0
    • Joined: 2019/04/17 09:28:54
    • Location: 0
    • Status: offline
    Re: Harmony v3 - No MCU's to select 2020/01/24 07:48:35 (permalink)
    0
    hi , i am facing the same issue 
     
    mplabx 5.30
    mhc 3.4.1 
    everything latest version
     
    did you manage to get a solution for this message ?
     
    #9
    ric
    Super Member
    • Total Posts : 28390
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: Harmony v3 - No MCU's to select 2020/01/25 13:43:05 (permalink)
    0
    Did you follow the steps in the couple of posts before yours?
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #10
    EngSam
    New Member
    • Total Posts : 18
    • Reward points : 0
    • Joined: 2019/04/17 09:28:54
    • Location: 0
    • Status: offline
    Re: Harmony v3 - No MCU's to select 2020/01/27 13:45:19 (permalink)
    0
    thank u 
    I have un-installed everything and repeat from scratch today and it works 
    maybe some package was updated , or maybe i installed the steps but not in the same order 
     
     
    #11
    Jump to:
    © 2020 APG vNext Commercial Version 4.5