• AVR Freaks

PIC IC malfunction

Author
m4l1c1ou5
New Member
  • Total Posts : 22
  • Reward points : 0
  • Joined: 2019/03/26 01:03:22
  • Location: 0
  • Status: offline
2019/06/16 12:40:19 (permalink)
0

PIC IC malfunction

will a PIC ic malfunction if burnt too many times? i.e if I am writing some code then it is not working perfectly as coded this behavior is mainly shown when I am defining variables.
I am using pic16f877a.
 
#1

3 Replies Related Threads

    jtemples
    عُضْوٌ جَدِيد
    • Total Posts : 11214
    • Reward points : 0
    • Joined: 2004/02/13 12:31:19
    • Location: Southern California
    • Status: offline
    Re: PIC IC malfunction 2019/06/16 12:50:08 (permalink)
    +1 (1)
    will a PIC ic malfunction if burnt too many times?

     
    Yes, but "too many" is a very large number and you haven't likely reached it.
    #2
    ric
    Super Member
    • Total Posts : 22725
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: PIC IC malfunction 2019/06/16 13:16:58 (permalink)
    +1 (1)
    m4l1c1ou5
    will a PIC ic malfunction if burnt too many times? i.e if I am writing some code then it is not working perfectly as coded this behavior is mainly shown when I am defining variables.
    I am using pic16f877a.
     

    It's much more likely a simpler problem, like:
    you have the Watchdog timer enabled, without code to feed it
    or have LVP enabled without a pulldown on RB3/PGM
    or, there's a bug in your program.

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #3
    katela
    Super Member
    • Total Posts : 1287
    • Reward points : 0
    • Joined: 2013/06/11 05:25:18
    • Location: South Africa
    • Status: offline
    Re: PIC IC malfunction 2019/06/16 14:14:19 (permalink)
    +1 (1)
    That PIC could be programmed probably more than 100 000 times ( the actual number could be in the datasheet ).
    In practice it's very unlikely to happen. The problem could be elsewhere as advised above.
    If you could describe the exact behavior you are experiencing and post your code, you might get more pointers to the problem.

    Free online Microcontroller Tutorials and Projects for Hobbyists and students. From beginners to advanced. Website: www.studentcompanion.co.za
    YouTube Tutorials: https://www.youtube.com/StudentCompanionSA
    #4
    Jump to:
    © 2019 APG vNext Commercial Version 4.5