• AVR Freaks

Hot!PIC16F1779 OPAxIN0- Pin not released when using unity gain

Author
OscarTheGrouch
Super Member
  • Total Posts : 308
  • Reward points : 0
  • Joined: 2010/11/29 18:07:28
  • Location: 0
  • Status: offline
2019/06/15 09:44:52 (permalink)
0

PIC16F1779 OPAxIN0- Pin not released when using unity gain

Hi all,
Doing a project with a PIC16F1779 using 4 DACs and the 4 OP Amps.
Positive input to them comes from DACs and FVR.
I click the check box for Unity Gain but still have to have a selection for the negative input.
Trying to use the pins associated with those inputs in pin manager for GPIO outputs gets a warning about
the conflict. Project compiles and works OK.
MAybe this could be fixed?
OtG
#1

1 Reply Related Threads

    PA91
    Junior Member
    • Total Posts : 70
    • Reward points : 0
    • Joined: 2012/09/03 21:45:40
    • Location: 0
    • Status: offline
    Re: PIC16F1779 OPAxIN0- Pin not released when using unity gain 2019/11/05 23:43:11 (permalink)
    0
    This issue has been resolved.
    Tested in "pic10-pic12-pic16-pic18-1.78.0"
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5