• AVR Freaks

Hot!Question:

Author
a.haas
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2019/06/12 03:30:20
  • Location: 0
  • Status: offline
2019/06/14 01:17:27 (permalink)
0

Question:

Hello, I am searching for a WiFi chip which is connected to PIC32 MX/MZ micro and the important thing is there is no free SPI interface available. There is only free UART interface and as I understood this will be used for debugging the WiFi chip only. Any idea how to connect on other way WiFi chip to this PIC32 MX/MZ?
Second Question: Both chips have an USB-Module, but with different variants. Is it maybe possible to connect both devices with an usb-wifi-module? Important thing is that the choosen device has Wifi-Direct and 150mpbs.
 
I would be glad, if someone could answer my questions. Thanks! 
 
Details:
PIC32MX460F512L
PIC32Z2064DAH176


#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5