• AVR Freaks

MHC Menu Empty

Author
UncleTom
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2009/11/24 06:27:07
  • Location: 0
  • Status: offline
2019/06/13 04:00:18 (permalink)
0

MHC Menu Empty

MPLAB Version 5.20 (same issue with 5.15) on MacOs
XC32 v2.20
Harmony Version 3
Harmony 3 Configurator (v3.3.0.1)
 
The MCH menu in the main tool bar doesn't contain any items. This means that when MHC is set to native mode (instead of standalone), a number of settings are missing (such as pin configuration). Have tried removing and re-installing the configurator plugin, but no fix. Can't find any obvious errors in the log files. Anybody else had this issue, or know how to resolve it? Or am I missing something and this menu doesn't actually have anything in it?
#1

0 Replies Related Threads

    Jump to:
    © 2019 APG vNext Commercial Version 4.5