• AVR Freaks

EERAM example with Harmony 2.xx (???)

Author
DominusT
Super Member
  • Total Posts : 1505
  • Reward points : 0
  • Joined: 2005/07/22 08:31:18
  • Status: offline
2019/06/12 08:49:29 (permalink)
0

EERAM example with Harmony 2.xx (???)

Hi.
 
Is there an example in Harmony (2.xx) to manage a EERAM with a PIC32MZ?
 
Thanks
#1
NKurzman
A Guy on the Net
  • Total Posts : 19194
  • Reward points : 0
  • Joined: 2008/01/16 19:33:48
  • Location: 0
  • Status: offline
Re: EERAM example with Harmony 2.xx (???) 2019/06/12 09:29:40 (permalink)
0
Serial? Parallel? I2C? SQI?
If it is I2C it should be similar to an EEPROM.
#2
DominusT
Super Member
  • Total Posts : 1505
  • Reward points : 0
  • Joined: 2005/07/22 08:31:18
  • Status: offline
Re: EERAM example with Harmony 2.xx (???) 2019/06/12 09:31:19 (permalink)
0
NKurzman
Serial? Parallel? I2C? SQI?
If it is I2C it should be similar to an EEPROM.


At the moment they are only I2C:

https://www.microchip.com...rs/memory/serial-eeram
#3
Jump to:
© 2021 APG vNext Commercial Version 4.5