• AVR Freaks

RN4871 Embedded scripting issue

Author
pacwin
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2019/06/05 15:31:01
  • Location: 0
  • Status: offline
2019/06/10 13:53:00 (permalink)
0

RN4871 Embedded scripting issue

Hello,
 
I can get my RN4871 module into command mode and send various different commands to it, which it accepts and replies to the ones i have tried.
 
When i input 'ww' to enter script input mode, i input a test script and then try and exit with typing 'ESC'. I cannot get the module to reply after exiting the script mode.
 
@PW_ON
|O,18,18
 
I power cycle the unit, which is when it responds to commands again. When sending the 'LW' command to display any stored scripted, nothing is shown.
 
Is there something i am doing wrong?
 
i have been through the manual a couple of times and tried a couple of difference examples to no avail.
 
Thanks,
#1

2 Replies Related Threads

    pacwin
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2019/06/05 15:31:01
    • Location: 0
    • Status: offline
    Re: RN4871 Embedded scripting issue 2019/06/13 14:42:17 (permalink)
    0
    I have managed to solve it, through trail and error.
     
    I was using ardunio serial monitor which was blocking the 'ESC' key from being sent over the UART. I switched tera term and worked fine. pressing 'ESC' does not need the /cr at the end either (cartridge return) like the '$$$' command. You should get 'CMD> AOK' received back after pressing 'ESC' key
     
    some examples give 'ESC' to be typed  but that does not work, you need to press the 'ESC' key
     
     
    #2
    extronic
    Starting Member
    • Total Posts : 33
    • Reward points : 0
    • Joined: 2018/09/06 00:10:53
    • Location: 0
    • Status: offline
    Re: RN4871 Embedded scripting issue 2019/06/21 14:31:23 (permalink)
    0
    It's good idea not to use Arduino ;) you've already found at least one reason why
    #3
    Jump to:
    © 2021 APG vNext Commercial Version 4.5