• AVR Freaks

ATWINC3400-MR210CA BT serial HW handshaking pins

Author
_fragment_
Super Member
  • Total Posts : 416
  • Reward points : 0
  • Joined: 2008/10/08 09:17:55
  • Location: Idaho
  • Status: online
2019/06/10 13:34:42 (permalink)
0

ATWINC3400-MR210CA BT serial HW handshaking pins

Page 8 of the data sheet shows pins 10 and 11 as I2C slave pins for test purposes only.
 
Page 34 shows a reference schematic with pin 10 as BT_RTS and pin 11 as BT_CTS connecting to the host processor.
 
So, which is it? Our hardware designer used the reference schematic. Now I'm developing the code and do not know if there are HW handshaking pins to code for or not. Anyone here have some insight?
 
Dave
#1

1 Reply Related Threads

    _fragment_
    Super Member
    • Total Posts : 416
    • Reward points : 0
    • Joined: 2008/10/08 09:17:55
    • Location: Idaho
    • Status: online
    Re: ATWINC3400-MR210CA BT serial HW handshaking pins 2019/06/17 16:07:34 (permalink)
    0
    It would appear that I'm blazing my own trail on this one, then?
     
    Dave
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5