• AVR Freaks

Hot!Harmony : Dual Memory SdCard Support ?

Author
TS9
Super Member
  • Total Posts : 841
  • Reward points : 0
  • Joined: 2010/05/07 10:52:22
  • Status: offline
2019/05/31 20:07:51 (permalink)
0

Harmony : Dual Memory SdCard Support ?

Hi,

I am planning use PIC32 (MX, MK or MZ) architecture with Harmony V2_06.

Can I use/access two different sdcards with Single SPI module and different Select Lines, and Should I go for two different SPI modules
with Harmony...
?

I need to copy the data from one SDCard to another .

Please suggest.




Thanks in advance.
--
TS9
post edited by TS9 - 2019/07/05 04:27:32
#1

6 Replies Related Threads

    TS9
    Super Member
    • Total Posts : 841
    • Reward points : 0
    • Joined: 2010/05/07 10:52:22
    • Status: offline
    Re: Harmony : Dual Memony SdCard Support ? 2019/06/04 01:57:10 (permalink)
    0
    Hi,
     
    I have checked Harmony V2_06 MHC Drivers Setting Tab .
     
    Number of USART Driver Instances available for USART
    Number of Timer Driver Instances  available for Timer.
     
    But SDCard Driver has not this option.....Number of SDCard Driver Instances ?
     
     
    Will it possible to Interface two microSDCard with Single SPI Module with different select lines with harmony ?
    According to my requirement I have to copy data from one microsdcard to another ?
     
    Please reply..
    --
    TS9
     

    Attached Image(s)

    #2
    Paul PortSol
    Super Member
    • Total Posts : 549
    • Reward points : 0
    • Joined: 2015/07/03 11:52:03
    • Location: Newfoundland, Canada
    • Status: offline
    Re: Harmony : Dual Memony SdCard Support ? 2019/06/04 04:54:39 (permalink)
    0
    I suggest you post a ticket to Microchip support.
    Also refer to Harmony Release notes and Errata for PIC's Datasheet, might be something there.
     
    #3
    TS9
    Super Member
    • Total Posts : 841
    • Reward points : 0
    • Joined: 2010/05/07 10:52:22
    • Status: offline
    Re: Harmony : Dual Memony SdCard Support ? 2019/07/05 04:26:39 (permalink)
    0
    Hi Paul ,
     
    Support team suggest me
    " To do this with the SD card driver, you will need to set the MHC setting "Number of SD Card Driver Clients" to 2. "
    1)
    Then what will be SPI Instance 1 or 2 ?
    2)
    Should that individual SPI (SPI1 and SPI2) or Single SPI with different select lines?
    3)
    Will harmony generate

    const DRV_SDCARD_INIT drvSDCardInit =
    {
    .spiId = SPI_ID_1,
    .spiIndex = 0,
    .sdcardSpeedHz = 1000000,
    .spiClk = CLK_BUS_PERIPHERAL_1,
    .chipSelectPort = PORT_CHANNEL_F,
    .chipSelectBitPosition = PORTS_BIT_POS_12,                 //?? What for 2nd SDCard..
    };

    4) How to both one by one...
     
     
    Could anybody help me for this?
    --
    TS9
     
     
    #4
    Paul PortSol
    Super Member
    • Total Posts : 549
    • Reward points : 0
    • Joined: 2015/07/03 11:52:03
    • Location: Newfoundland, Canada
    • Status: offline
    Re: Harmony : Dual Memony SdCard Support ? 2019/07/05 04:53:39 (permalink)
    0
    Best resolve this with support team.
    Maybe they can provide a simple sample project (that you can share here)
     
    #5
    TS9
    Super Member
    • Total Posts : 841
    • Reward points : 0
    • Joined: 2010/05/07 10:52:22
    • Status: offline
    Re: Harmony : Dual Memony SdCard Support ? 2019/07/05 05:33:51 (permalink)
    0
    Paul PortSol
    Best resolve this with support team.Maybe they can provide a simple sample project (that you can share here) 

    Thanks...I will surely get in Touch with them..
    #6
    TS9
    Super Member
    • Total Posts : 841
    • Reward points : 0
    • Joined: 2010/05/07 10:52:22
    • Status: offline
    Re: Harmony : Dual Memory SdCard Support ? 2019/08/09 22:15:25 (permalink)
    0
    Hi,
     
    After Some search over microchip website.. I got the link the H3 can support dual microSDCard but with
    different SPI Channels (0 and 1).
     
    Screenshot attached ..Have any body tried that?
     
    --
    TS9

    Attached Image(s)

    #7
    Jump to:
    © 2020 APG vNext Commercial Version 4.5