• AVR Freaks

I have a problem with upgrading RN-171 from 4.41 to 4.75 by its "timeout"

Author
tomi
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2019/05/16 23:18:04
  • Location: 0
  • Status: offline
2019/05/31 18:01:07 (permalink)
0

I have a problem with upgrading RN-171 from 4.41 to 4.75 by its "timeout"

Please give me advise, how to upgrade the firmware of RN-171 from 4.41 to 4.75.
When I do ftp cu wifly7-475.mif , it indicates "timeout=2" after trying to connect ftp server.
I tried several network to do but the result was the same.
Does anybody know how to avoid its timeout?
 
Here is the procedure what I have done;
 
 
<4.41>
<4.41> set wlan ssid HG8045-B59D-bg
AOK
<4.41> set wlan phrase xxxxxxxxxxxxxxx
AOK
<4.41> join
<4.41> Auto-Assoc HG8045-B59D-bg chan=5 mode=MIXED SCAN OK
Joining HG8045-B59D-bg now..
Associated!
DHCP: Start
DHCP in 5072ms, lease=86400s
IF=UP
DHCP=ON
IP=192.168.1.36:2000
NM=255.255.255.0
GW=192.168.1.1
Listen on 2000

<4.41> ftp cu wifly7-475.mif
 del  5 config
<4.41> FTP connecting to 198.175.253.161
FTP timeout=2
 
----------------------------------------------------------
For more reference;
I have checked ftp as follows;
 
 
<4.41>
<4.41> get ftp
FTP=198.175.253.161:21
File=wifly-EZX.img
User=roving
Pass=Pass123
Dir=public
Timeout=200
FTP_mode=0x0
<4.41>
 
post edited by tomi - 2019/06/05 22:48:41
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5