• AVR Freaks

Hot!ICD3 cannot program into device

Author
jainchen2
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2019/05/28 09:31:25
  • Location: 0
  • Status: offline
2019/05/29 09:05:03 (permalink)
0

ICD3 cannot program into device

I use ICD3 and MPLAB X IDE v3.55.  The ICD3 driver was downloaded correctly.  In Device Manager, it shows "Microchip WinUSB Device".
After I press "Make and Program Device" button in IDE, after make process, the ICD3 shows "Reception on endpoint 1 failed (err=-10031).  Connection Failed."
What should I do?

Attached Image(s)

#1

2 Replies Related Threads

    NKurzman
    A Guy on the Net
    • Total Posts : 18260
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: ICD3 cannot program into device 2019/05/29 10:50:08 (permalink)
    0
    Windows? Linux? A Mac? What version?
    Did it work before or is it a new installation?
    #2
    NorthGuy
    Super Member
    • Total Posts : 5917
    • Reward points : 0
    • Joined: 2014/02/23 14:23:23
    • Location: Northern Canada
    • Status: online
    Re: ICD3 cannot program into device 2019/05/29 12:07:50 (permalink)
    0
    That's an USB problem. Try connecting it to a different USB socket on your PC. If it persists all the time, contact Microchip. They'll replace your ICD3 under warranty.
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5