• AVR Freaks

Hot!Imposible change BLE Device Name BM64

Author
c.alonso
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2019/05/27 06:37:14
  • Location: 0
  • Status: offline
2019/05/29 00:45:07 (permalink)
0

Imposible change BLE Device Name BM64

Hi,
I'm trying to change the BLE Device Name of the BM64 through commands. I'm using the SPKCommandSetTool in order to test it and the name does not change.
I follow these steps:
  1. Disable Advertising
  2. Update Device Name
  3. Enable Advertising
I tried different options but I could not change the BLE Device Name.

 
Do you have any idea how can I solve it?
Regards

Attached Image(s)

#1

1 Reply Related Threads

    JustPlaneD
    New Member
    • Total Posts : 15
    • Reward points : 0
    • Joined: 2018/10/24 13:44:38
    • Location: 0
    • Status: offline
    Re: Imposible change BLE Device Name BM64 2019/08/14 15:50:31 (permalink)
    0
    Cycle the power to the Bluetooth radio on your Client device (Phone or Tablet). Many attributes are remembered based on the first time the device was discovered/connected. Cycling the power will make the Client device forget all of the stored information and it will reaquire the "new" data.
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5