• AVR Freaks

Hot!So I just found the USB-UART function on the DM182026 PIC18F46K42 Evaluation Board

Author
oliverb
Super Member
  • Total Posts : 206
  • Reward points : 0
  • Joined: 2009/02/16 13:12:38
  • Location: 0
  • Status: offline
2019/05/24 12:28:54 (permalink)
0

So I just found the USB-UART function on the DM182026 PIC18F46K42 Evaluation Board

In hindsight the extra COM port appearing in Device manager should have been a clue, and it is clearly stated that the "GENERAL PURPOSE EVALUATION BOARD" version includes a USB UART but you can see the specific PIC pins on the schematic, but I only just found out that the DM182026 version also provides a USB-UART function, this time using RB6 and RB7.
#1

0 Replies Related Threads

    Jump to:
    © 2019 APG vNext Commercial Version 4.5