• AVR Freaks

AnsweredBug? MCC Clock Diagram always loads FRCDIV=DIV_1

Author
chris_trenton
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2019/04/16 07:20:25
  • Location: 0
  • Status: offline
2019/05/23 05:59:48 (permalink)
0

Bug? MCC Clock Diagram always loads FRCDIV=DIV_1

Every time I open MPLAB Code Configurator (MCC) the "Clock Diagram" forces the value of FRCDIV to DIV_1.  I change the value, save the project, close MCC, re-open MCC, and I find FRCDIV is still DIV_1.  The defect is 100% repeatable over two different installs and many (many) different projects.  I have attached one such project to this post.
 
I open MCC this way: I ensure the project I intend to work with is set as "Main Project".  I use the "Tools > Embedded > MPLAB Harmony Configurator" menu option.  When the plugin prompts me, I verify the plugin being loaded is the MHC file associated with my project.
 
These are my tool versions:
  • Host: Win 10 x64
  • MPLAB X IDE v5.20 (also seen in v5.15)
  • MPLAB Code Configurator version 3.75
  • PIC32MZ2048EFM144
Has anyone else encountered this problem?  Is there anything more I can provide to help explore the issue?  This not not an urgent problem, but it is so pervasive in all my PIC32MZ projects that I felt compelled to learn if others encountered it.
 
-Chris
#1
arpananand
Super Member
  • Total Posts : 403
  • Reward points : 0
  • Joined: 2009/11/18 04:35:42
  • Location: 0
  • Status: offline
Re: Bug? MCC Clock Diagram always loads FRCDIV=DIV_1 2019/05/23 23:30:31 (permalink)
0
are you using Harmony or MCC? your attached file suggests Harmony but you have mentioned MCC in your post. if Harmony, then tell the correct version of Harmony you are using?
#2
chris_trenton
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2019/04/16 07:20:25
  • Location: 0
  • Status: offline
Re: Bug? MCC Clock Diagram always loads FRCDIV=DIV_1 2019/05/24 09:21:01 (permalink)
0
Pardon my confusion.  I had thought "MPLAB Harmony Configurator" and "MPLAB Code Configurator" were two different names for the same product--a rebranding.  Now I see I they are distinct plugins.  The "MPLAB Harmony Configurator" is the one I am interested in.  I use version 2.0.5.2.
 
Thanks for taking the time to clarify my question.  It cleared up something I did not even know to ask.
#3
arpananand
Super Member
  • Total Posts : 403
  • Reward points : 0
  • Joined: 2009/11/18 04:35:42
  • Location: 0
  • Status: offline
Re: Bug? MCC Clock Diagram always loads FRCDIV=DIV_1 2019/05/27 20:32:26 (permalink) ☼ Best Answerby chris_trenton 2019/05/29 10:17:59
0
Harmony v2 does have this issue. it has been fixed in Harmony v3, which you can find it here:
https://www.microchip.com/mplab/mplab-harmony/mplab-harmony-v3
 
#4
Jump to:
© 2019 APG vNext Commercial Version 4.5