• AVR Freaks

Hot!RN4871 non-bondable mode

Author
emathana
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2019/05/21 07:02:25
  • Location: Cyprus
  • Status: offline
2019/05/22 06:25:36 (permalink)
0

RN4871 non-bondable mode

According to the following
 
https://microchipdevelope...:ble-gap-security#toc1
 
There should be an option to completely disable the bonding ability of the module, but I have not found anything inside the manual of the RN4871 -C version. I am using the 1.30 firmware.
 
In the 1.18 firmware once paired (bonded) the device would refuse any connection. I saw in another thread that there is a beta firmware that addresses some of these issues. Does anyone have this firmware referenced here:
https://www.microchip.com/forums/m1053482.aspx
 
I am using the SA,2 command that indicates NoInputNoOutput mode.
 
Thank you in advance
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5