• AVR Freaks

Harmony V3 select a BSP.

Author
bordlab
Starting Member
  • Total Posts : 57
  • Reward points : 0
  • Joined: 2018/01/29 06:45:53
  • Location: 0
  • Status: offline
2019/05/21 12:56:26 (permalink)
0

Harmony V3 select a BSP.

I installed Harmony 3 with MPLAB v5.20.  When through the setup created my project.  Opened Harmony Configurator.  Then I want to add in a microchip development board instead of the Default Board (BSP).  When I drop it on my project graph and look at the options there is no where to change the BSP that is points to.  Where do I find this option in Harmony v3?
#1
Jump to:
© 2020 APG vNext Commercial Version 4.5