• AVR Freaks

Hot!SAMR34 Xplained pro IDE setup

Author
Udhayakumar
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2019/05/17 06:17:37
  • Location: 0
  • Status: offline
2019/05/17 19:09:46 (permalink)
0

SAMR34 Xplained pro IDE setup

Hi,
I recently I bought a SAMR34 Xplained pro kit. Following the user guide I installed Atmel studio 7 and updated ASF extension to latest 3.46 Version under "Extensions and Updates". but in the device example list there is no SAMR34 listed. I connected the SAMR34 kit and updated board details (Option displayed when board is connected) but then also in the ASF kit list SAMR34 is not listed but this the method mentioned in SAMR34 user guide. I have tried another option, File->New->Atmel Start Example Project, there also this specific device is not getting listed. I have attached snapshots here. 
 
Do I miss any updates here. How do I compile code for SAMR34?

Attached Image(s)

#1

1 Reply Related Threads

    katlin
    New Member
    • Total Posts : 10
    • Reward points : 0
    • Joined: 2019/12/23 01:32:03
    • Location: 0
    • Status: offline
    Re: SAMR34 Xplained pro IDE setup 2020/04/28 21:49:58 (permalink)
    0
    Please find the Step by Step Procedure here.
    https://docs.google.com/d...oKmZg/edit?usp=sharing
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5