• AVR Freaks

Does Harmony v3.0 have educational training material on the graphics library?

Author
PSIR
New Member
  • Total Posts : 29
  • Reward points : 0
  • Joined: 2018/05/27 19:05:17
  • Location: 0
  • Status: offline
2019/05/12 19:19:52 (permalink)
0

Does Harmony v3.0 have educational training material on the graphics library?

Currently on the Harmony website is v2.06:
Https://www.microchip.com/mplab/mplab-harmony

The old Graphics Library has the HIF2131 training course. I don't know whether the new version of Harmony v3.0 has an educational training manual for the graphics library.

Harmony v2.06's external graphics resource example is to use the USB Host mode, first put the graphics resource HEX file on the USB Disk, the MCU reads the HEX file and then writes to the SPI Flash, but when the MCU can only work in the Device mode,  v2.06 does not have Bootloader PC APP for Device mode. I hope Harmony v3.0 can develop the Bootloader for PC to write SPI Flash with graphics resources.
 
Especially in multi-language, V2.06 can edit several multi-language languages on the IDE, but how to switch flexibly does not know which functions to use, so I hope that there are detailed multi-language teaching in the training materials. About how to Management instructions.
 
Best Regard
#1

0 Replies Related Threads

    Jump to:
    © 2019 APG vNext Commercial Version 4.5