• AVR Freaks

Hot!Lr645lg transformerless power supply

Author
Aville
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2019/05/02 05:48:06
  • Location: 0
  • Status: offline
2019/05/11 15:33:00 (permalink)
0

Lr645lg transformerless power supply

Hello. Did anybody make the lr645 circuit with depletion mode mosfet(like in datasheet)? I tried but either mosfet is burning or lr645lg is burning.
Solved: problem was voltage regulator.
post edited by Aville - 2019/06/07 14:15:19
#1

2 Replies Related Threads

    oliverb
    Super Member
    • Total Posts : 206
    • Reward points : 0
    • Joined: 2009/02/16 13:12:38
    • Location: 0
    • Status: offline
    Re: Lr645lg transformerless power supply 2019/05/24 11:22:31 (permalink)
    5 (1)
    Can you elaborate on what you mean by that? Do you mean it is burning out or just running extremely hot?
     
    It is a linear regulator so running from high voltage the dissipation will be high. For a UK SMPS (>350V bus) the dissipation at 3mA would exceed 1W
     
     
     
    #2
    PStechPaul
    Super Member
    • Total Posts : 2381
    • Reward points : 0
    • Joined: 2006/06/27 16:11:32
    • Location: Cockeysville, MD, USA
    • Status: offline
    Re: Lr645lg transformerless power supply 2019/05/24 20:29:01 (permalink)
    4.5 (2)
    The OP has posted the exact same question in several forums and also in an old thread which has a little more information:
    https://www.microchip.com/forums/m927264.aspx
     
    However, we need to see a complete schematic of the OP's circuit, including input voltage and output load, as well as circuit layout and heat sinks for the power dissipating components.

     
    #3
    Jump to:
    © 2019 APG vNext Commercial Version 4.5