• AVR Freaks

Hot!RN4678 Transmit Power

Author
AnujKumar Satish
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2019/05/07 12:56:05
  • Location: 0
  • Status: offline
2019/05/08 09:04:11 (permalink)
0

RN4678 Transmit Power

In RN4678 Command sheet - 
The "SY <0-4>" ASCII command is used to set the transmit power level. Is 0 the highest transmit power or is 4 the highest? What are the transmit power levels associated with parameters 0-4
#1

3 Replies Related Threads

    RodMcM
    New Member
    • Total Posts : 7
    • Reward points : 0
    • Joined: 2016/04/27 18:34:26
    • Location: 0
    • Status: offline
    Re: RN4678 Transmit Power 2019/08/15 22:41:47 (permalink)
    0
    Hi
    An app I made tested RSSI as following after connection
    0       -62
    1       -57
    2       -65
    3       -59
    4       -69
    Not exactly a firm answer. I saw the RSSI readings higher during some period of the connection but cant capture them. These are the final connection values
    #2
    love.kull
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2019/09/16 03:19:05
    • Location: 0
    • Status: offline
    Re: RN4678 Transmit Power 2019/09/20 03:56:32 (permalink)
    0
    Hi
     
    So did you get any more insights about this?
     
    Best regards, L
    #3
    HFP
    New Member
    • Total Posts : 1
    • Reward points : 0
    • Joined: 2019/11/11 05:49:31
    • Location: 0
    • Status: offline
    Re: RN4678 Transmit Power 2019/11/11 23:17:11 (permalink)
    0
    I've done some similar tests yesterday, just to be sure about this question.
     
    But in opposite to the former values in this forum thread here, my RSSI levels were much better.
     
    Mybe the pure distance (less than a single meter beside the notebook) but probably my antenna ground plane construction (exactly as recommended in the data sheet).
     
    In a few words, RSSI values with SY,1 were mostly within -20 to -10 range (I've played a little bit with additional walls in the line of sght), and clearly increased to values between -5 and 0 with SY,4 ... :-)
     
    Cheers!
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5