• AVR Freaks

Hot!How do I set the start folder that starts every time I add existing object to project?

Author
user2x
Super Member
  • Total Posts : 224
  • Reward points : 0
  • Joined: 2011/02/10 20:43:36
  • Location: 0
  • Status: offline
2019/05/02 18:27:19 (permalink)
0

How do I set the start folder that starts every time I add existing object to project?

Hello,
 
Every time I want to add an existing file to my new project (Right click - add existing), it starts in the .X folder somewher and I have to click a number of time out of there and into the .src folder I have.
 
How do I set the folder to not start in the .X folder every time?
 
Regards
X
#1

6 Replies Related Threads

    aschen0866
    Super Member
    • Total Posts : 4434
    • Reward points : 0
    • Joined: 2006/01/08 22:18:32
    • Location: San Diego
    • Status: offline
    Re: How do I set the start folder that starts every time I add existing object to project? 2019/05/02 19:04:48 (permalink)
    +1 (1)
    I don't know if there is a way to change this behavior. If I am creating a new project, I usually use "Add Existing Items from Folders..." and it seems to remember the last folder location.
    #2
    hkv
    Starting Member
    • Total Posts : 15
    • Reward points : 0
    • Joined: 2018/08/06 10:11:49
    • Location: 0
    • Status: offline
    Re: How do I set the start folder that starts every time I add existing object to project? 2019/05/20 15:26:17 (permalink)
    0
    Right click on top of the folder where you want add the file(the desired folder would be highlighted), then choose add existing item if its a file that needs to be added. In case it's a folder choose add existing items from folder. Doing that would add the file in the desired folder.
    #3
    hkv
    Starting Member
    • Total Posts : 15
    • Reward points : 0
    • Joined: 2018/08/06 10:11:49
    • Location: 0
    • Status: offline
    Re: How do I set the start folder that starts every time I add existing object to project? 2019/05/20 15:26:17 (permalink)
    0
    Right click on top of the folder where you want add the file(the desired folder would be highlighted), then choose add existing item if its a file that needs to be added. In case it's a folder choose add existing items from folder. Doing that would add the file in the desired folder.
    #4
    user2x
    Super Member
    • Total Posts : 224
    • Reward points : 0
    • Joined: 2011/02/10 20:43:36
    • Location: 0
    • Status: offline
    Re: How do I set the start folder that starts every time I add existing object to project? 2019/05/20 17:15:01 (permalink)
    0
    That is not exactly what I am asking as such.
     
    What you write is correct but that very first folder location that pops up when you add existing file / item...
    How do I set where that starts? Mine starts way off in a far out different folder every time and I need to click through heaps of folders to get to the file I want to add. That happens every single time I want to add a file.


     
     
    #5
    hkv
    Starting Member
    • Total Posts : 15
    • Reward points : 0
    • Joined: 2018/08/06 10:11:49
    • Location: 0
    • Status: offline
    Re: How do I set the start folder that starts every time I add existing object to project? 2019/05/20 17:32:29 (permalink)
    0
    Is it totally out of the folder where your project is(like a completely different folder where your project doesn't actually exist)?
    Or does it start from the folder where the last files were added?
    #6
    user2x
    Super Member
    • Total Posts : 224
    • Reward points : 0
    • Joined: 2011/02/10 20:43:36
    • Location: 0
    • Status: offline
    Re: How do I set the start folder that starts every time I add existing object to project? 2019/05/20 18:04:32 (permalink)
    0
    It ALWAYS starts in the same folder. Not the one I last used. that is the whole problem.
     
    The folder is in the .X project folder somewhere.   I do not have it open as I type here so I can't tell the exact folder. 
    #7
    Jump to:
    © 2019 APG vNext Commercial Version 4.5