• AVR Freaks

Hot!Will there be a real ice 2?

Author
seyyah
Super Member
  • Total Posts : 609
  • Reward points : 0
  • Joined: 2004/05/14 12:49:28
  • Status: offline
2019/04/30 06:56:27 (permalink)
0

Will there be a real ice 2?

I've been using this device for over 10 years, I cannot believe how still Microchip can sell this very problematic, very expensive and clumsy device? Instead of debugging the project, I'm trying to solve the real ice problems, pray it not to fall into an error or halt or lost connection or give errors like:
 
An Error occurred while running
Failed while sending cmd_SET_PERIPHERAL_FREEZE command
Invalid command response (sent 0x71, received 0x3f)
Failed getting PC
FAILED_SETTING_SWBP
Invalid command response (sent 0x3f, received 0x89)
 
It's tough to create the scenario and catch the bug in the program most of the time, just when the real ice is needed it fails and gives some stupid error! What a shame!
#1

5 Replies Related Threads

    du00000001
    Just Some Member
    • Total Posts : 2687
    • Reward points : 0
    • Joined: 2016/05/03 13:52:42
    • Location: Germany
    • Status: online
    Re: Will there be a real ice 2? 2019/04/30 07:00:27 (permalink)
    +2 (2)
    Are you really convinced that it's the "clumsy tool" and not the clumsy user?
    I do not experience problems - even with the latest PICs...
    post edited by du00000001 - 2019/05/22 03:29:30

    PEBKAC / EBKAC / POBCAK / PICNIC (eventually see en.wikipedia.org)
    #2
    KTrenholm
    Super Member
    • Total Posts : 707
    • Reward points : 0
    • Joined: 2012/08/08 14:04:23
    • Location: Connecticut, USA
    • Status: offline
    Re: Will there be a real ice 2? 2019/04/30 07:10:29 (permalink)
    +1 (1)
    Hmm, I've never seen that set of errors before on my ICE.
    Wonder if maybe it's a PC->ICE connection issue?
    OP, check you're using a decent USB cable and if not doing so already, connect directly to the PC as hubs can sometimes cause issues communicating with the tool.
     
    If connection issues are ruled out and you still run into problems it would probably be worth opening a ticket with Microchip.
    #3
    Jim Nickerson
    User 452
    • Total Posts : 5956
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: offline
    Re: Will there be a real ice 2? 2019/04/30 08:00:12 (permalink)
    0
    I also have not seen these errors on my ICE.
    #4
    NKurzman
    A Guy on the Net
    • Total Posts : 17361
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: Will there be a real ice 2? 2019/04/30 08:30:19 (permalink)
    0
    What Version of MPLab?  Which PIC?
     
    #5
    seyyah
    Super Member
    • Total Posts : 609
    • Reward points : 0
    • Joined: 2004/05/14 12:49:28
    • Status: offline
    Re: Will there be a real ice 2? 2019/05/22 02:27:24 (permalink)
    0
    I have used nearly all series of pics except the latest pic32mz and mk. All versions of mplabs since v6 or olders but real ice with V8. I have used may be a dozen computers including desktops and laptops. I've used several windows OSes. I have used a lot of different usb cables and tried usb hubs. I also purchased performance pack. I've tried several real ices. It was always problematic. If the problem is me, what am I doing wrong and I still could not solve for over 10 years?
    #6
    Jump to:
    © 2019 APG vNext Commercial Version 4.5