• AVR Freaks

MPLABx IDE not starting

Author
AndersG
Super Member
  • Total Posts : 200
  • Reward points : 0
  • Joined: 2008/08/05 04:51:24
  • Location: 0
  • Status: offline
2019/04/17 01:13:14 (permalink)
0

MPLABx IDE not starting

Just noticed it and was at 5.05, tried installing 5.15 and it is the same thing. It gets as far as "Done Loading Modules" and then just exits. I have tied clearing the persistence files. Does not help. Same goes for the older 3.x and 5.x versions I have installed.
 
I have attached the log. Any ideas?
 
Edit: Installed on another machine and compared logs. The failing machine's last entry is "Internet connection detected." the working machine continues after that.
 
edit: This affects IPE as well. Dies just after it establishes network connectivity. The windows FW asks  if it is OK to connect and the it dies.
post edited by AndersG - 2019/04/17 08:43:22

Attachment(s)

Attachments are not available: Download requirements not met
#1

2 Replies Related Threads

    AndersG
    Super Member
    • Total Posts : 200
    • Reward points : 0
    • Joined: 2008/08/05 04:51:24
    • Location: 0
    • Status: offline
    Re: MPLABx IDE not starting 2019/04/18 06:04:54 (permalink)
    0
    Apparently related to MicroFocus Filr. I have opened a case with Microchip (
    00406817) and with Microfocus.
    #2
    AndersG
    Super Member
    • Total Posts : 200
    • Reward points : 0
    • Joined: 2008/08/05 04:51:24
    • Location: 0
    • Status: offline
    Re: MPLABx IDE not starting 2019/04/28 03:06:06 (permalink)
    0
    Just to close the loop. I got excellent support from both Microchip and MicroFocus and now have a workaround that lets me use both Filr and MPLABx
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5