• AVR Freaks

Hot!Wrong window visualization for Comparator / Op-Amps / Volt Ref block

Author
FilippoMonti
Starting Member
  • Total Posts : 32
  • Reward points : 0
  • Joined: 2017/11/03 03:10:15
  • Location: 0
  • Status: offline
2019/04/16 06:40:18 (permalink)
0

Wrong window visualization for Comparator / Op-Amps / Volt Ref block

 
Dear Lubin,
 
I have a PC with 13" FHD screen. So that by default on windows properties there is a 150% zoom for the correct visualization on my screen.
With these properties I cannot see correctly the window of the Comparator / Op amp block. I see only the bottom part and I cannot scroll to the top.
Only by setting 100% magnitude I can see it correctly but then I see all out of focus.
 
For the next release, is it possible to implement the possibility to scroll within the block menu?
With other blocks all is ok.
 
Thank you
 
Filippo

Attached Image(s)

#1

4 Replies Related Threads

    Lubin
    Moderator
    • Total Posts : 387
    • Reward points : 5
    • Joined: 2007/03/31 07:38:15
    • Location: Bayonne, France
    • Status: offline
    Re: Wrong window visualization for Comparator / Op-Amps / Volt Ref block 2019/04/16 09:17:03 (permalink)
    0
    Hi Filippo,
     
    Thanks for your feedback.
    Using such tiny screen to work with simulink is not very common.
     
    We'll see if a GUI improvement is feasible for this block GUI.  I am not sure it is that easy.
    In any case, we'll take this in consideration for futur blocks.
     
    Lubin
    #2
    FilippoMonti
    Starting Member
    • Total Posts : 32
    • Reward points : 0
    • Joined: 2017/11/03 03:10:15
    • Location: 0
    • Status: offline
    Re: Wrong window visualization for Comparator / Op-Amps / Volt Ref block 2019/04/17 02:38:07 (permalink)
    0
    Hi Lubin,
     
    sorry for bother you further but, I cannot see the option "block output" for the outputs of the op amps. While I see the tab for the comparators.
     
    Is it normal? how can I receive in Simulink the output from the op amps?
     
    Thank you
     
    Filippo
    #3
    Lubin
    Moderator
    • Total Posts : 387
    • Reward points : 5
    • Joined: 2007/03/31 07:38:15
    • Location: Bayonne, France
    • Status: offline
    Re: Wrong window visualization for Comparator / Op-Amps / Volt Ref block 2019/04/17 03:56:12 (permalink)
    0
    The Comparator Op-Amp block configure the onboard Op-Amp - Comparator module.
     
    Result of the Op-Amp is an analog voltage you can find on your board.
    The Op-Amp output is also an input for the ADC.
     
    Thus you get the Op-Amp "output" value through the ADC block. Select an input pin which is your Op-Amp output pin.
     
    #4
    FilippoMonti
    Starting Member
    • Total Posts : 32
    • Reward points : 0
    • Joined: 2017/11/03 03:10:15
    • Location: 0
    • Status: offline
    Re: Wrong window visualization for Comparator / Op-Amps / Volt Ref block 2019/04/17 07:13:15 (permalink)
    0
    Dear Lubin,
     
    thank you. very helpful :)
     
    Filippo
    #5
    Jump to:
    © 2019 APG vNext Commercial Version 4.5