• AVR Freaks

Hot!Harmony 3 support for PIC32MX ?

Author
GrahamH
Junior Member
  • Total Posts : 102
  • Reward points : 0
  • Joined: 2010/04/23 20:37:12
  • Location: Austin, TX
  • Status: offline
2019/04/12 07:15:49 (permalink)
0

Harmony 3 support for PIC32MX ?

I note that the PIC32MX is not supported in the current download of Harmony 3, only PIC32MZ and MK.
 
Will the PIC32MX be added?
Or is PIC32MX recommended to use 2.06 for Harmony framework, rather than Harmony 3?
 
Is the current Harmony 2.06 the last planned release for Harmony 2?
 
I am trying to do some migration planning for some older products using PIC32MX.
 
--- Graham
 
==
#1

12 Replies Related Threads

    JPortici
    Super Member
    • Total Posts : 668
    • Reward points : 0
    • Joined: 2012/11/17 06:27:45
    • Location: Grappaland
    • Status: offline
    Re: Harmony 3 support for PIC32MX ? 2019/04/12 07:21:51 (permalink)
    #2
    Jim Nickerson
    User 452
    • Total Posts : 5892
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: offline
    nigelwright7557
    Super Member
    • Total Posts : 208
    • Reward points : 0
    • Joined: 2006/11/06 08:15:51
    • Location: 0
    • Status: offline
    Re: Harmony 3 support for PIC32MX ? 2019/04/12 07:58:54 (permalink)
    0
    I have done a couple of projects using pic32mx and harmony with no problems.
    I use USB and A2D.
    #4
    Tim Cruise
    Junior Member
    • Total Posts : 91
    • Reward points : 0
    • Status: offline
    Re: Harmony 3 support for PIC32MX ? 2019/04/12 09:55:19 (permalink)
    0
    We should not chase the latest IDE version for every project.
     
    For instance, I am testing a new project on PIC32MZEF which requires no graphics.  I find that Harmony 2.06 works better.  Harmony 3 is too complicated though.
    #5
    GrahamH
    Junior Member
    • Total Posts : 102
    • Reward points : 0
    • Joined: 2010/04/23 20:37:12
    • Location: Austin, TX
    • Status: offline
    Re: Harmony 3 support for PIC32MX ? 2019/04/12 12:34:10 (permalink)
    0
    Jim Nickerson said:
    >> Have you seen this https://github.com/Microc...io/wiki/device_support
     
    Thanks, Jim.
    I think I know what "Yes" means.
    A blank box, I guess, is the absence of "Yes"
    That implies "No", but could mean "not at this time, coming soon" or could mean "no, not ever", or probably means "end of support for the PIC32MX."
     
    I am just trying to plan the firmware migration path for some existing shipping products that use the PIC32MX, that need some serious bug-fixing and feature addition.
     
    --- Graham
     
    ==
    #6
    Jim Nickerson
    User 452
    • Total Posts : 5892
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: offline
    Re: Harmony 3 support for PIC32MX ? 2019/04/13 07:36:07 (permalink)
    0
    Graham,
    My best guess is they are concentrating on adding support for devices not in 2.06 and these new devices require different underlying infrastructure.
    As the Mx devices are already supported in 2.06 and 3. is still in beta I would guess the blanks indicate they will be supported.
    I am not a Microchip employee and have no inside information, just my guess.
    #7
    MikeinAZ
    Administrator
    • Total Posts : 309
    • Reward points : 0
    • Joined: 2014/06/03 07:25:32
    • Location: Chandler, AZ
    • Status: offline
    Re: Harmony 3 support for PIC32MX ? 2019/04/15 10:01:53 (permalink)
    5 (2)
    I want to address the concern generally.
    Yes, we have plans to release PIC32MX support in Harmony 3.  You are all correct that we do not have this in there yet.  The plan was first to address much of the Cortex family, then add classic MCHP (MIPS based) devices as we move forward.  We are in this second phase now.
    PIC32MX is a larger tent, with a number of device families.  So we are starting with several that should be done within this quarter, but others will follow later.
    With multiple repositories please also be aware that we generally focus on CSP and Core functions first, and in some cases middleware will follow on later.
    Lastly, we are also planning another Harmony v2.xx (v2.07 is next) support round in the second half of the year.  So if you are on Harmony 2 and it is working for you for a given family, it will continue to have some support.
    #8
    Jim Nickerson
    User 452
    • Total Posts : 5892
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: offline
    Re: Harmony 3 support for PIC32MX ? 2019/04/15 10:05:52 (permalink)
    0
    Mike,
    Thank you for clearing that up.
    It is always nice to know the roadmap.
    #9
    TS9
    Super Member
    • Total Posts : 651
    • Reward points : 0
    • Joined: 2010/05/07 10:52:22
    • Status: offline
    Re: Harmony 3 support for PIC32MX ? 2019/04/15 11:25:09 (permalink)
    0
    MikeinAZ
    I want to address the concern generally.Yes, we have plans to release PIC32MX support in Harmony 3.  You are all correct that we do not have this in there yet.  The plan was first to address much of the Cortex family, then add classic MCHP (MIPS based) devices as we move forward.  We are in this second phase now.PIC32MX is a larger tent, with a number of device families.  So we are starting with several that should be done within this quarter, but others will follow later.With multiple repositories please also be aware that we generally focus on CSP and Core functions first, and in some cases middleware will follow on later.Lastly, we are also planning another Harmony v2.xx (v2.07 is next) support round in the second half of the year.  So if you are on Harmony 2 and it is working for you for a given family, it will continue to have some support.

    When Harmony 3 will support File
    Systems microSDs and sd_msd_multi_fs ?

    Thanks
    #10
    TS9
    Super Member
    • Total Posts : 651
    • Reward points : 0
    • Joined: 2010/05/07 10:52:22
    • Status: offline
    Re: Harmony 3 support for PIC32MX ? 2019/04/15 23:53:16 (permalink)
    0
    Will Harmony 3 File System Supports exFAT for more than 32GB microSDCards and USB  Flash drives ?
    #11
    GrahamH
    Junior Member
    • Total Posts : 102
    • Reward points : 0
    • Joined: 2010/04/23 20:37:12
    • Location: Austin, TX
    • Status: offline
    Re: Harmony 3 support for PIC32MX ? 2019/04/17 12:01:44 (permalink)
    0
    Mike:
    Thanks for the clarification.
    That helps me understand where Microchip is headed.
    --- Graham
    #12
    MikeinAZ
    Administrator
    • Total Posts : 309
    • Reward points : 0
    • Joined: 2014/06/03 07:25:32
    • Location: Chandler, AZ
    • Status: offline
    Re: Harmony 3 support for PIC32MX ? 2019/04/23 09:07:35 (permalink)
    0
    Please use a new thread to change the topic.  You will get more attention that way.
     
    Currently we are only porting existing structures primarily from Harmony 2, but others may include content from ASF or other Cortex libraries / sources.  This includes the file system.
     
    Over time of course things can change, but FS updates are not a major feature request.  We do not plan on file system updates in the near future.
     
    You can always put in a support ticket to request these items, or communicate in the 'issues' section of GitHub.  We are interested in customer feedback like this.  
    #13
    Jump to:
    © 2019 APG vNext Commercial Version 4.5