• AVR Freaks

Hot!MPLAB X 5.65 doesn't find JAVA

Author
_Claudia
New Member
  • Total Posts : 6
  • Reward points : 0
  • Joined: 2010/02/18 14:22:37
  • Location: 0
  • Status: offline
2019/04/11 08:28:51 (permalink)
0

MPLAB X 5.65 doesn't find JAVA

Hi guys,
I have downloaded and installed MPLAB X IDE V5.65 for Windows (x86/x64) on my pc running Win10 OS (AMD Quad-core processor) and JAVA 8 (jre1.8.0_201).  (I installed Java before MPLAB)
When I try to lunch MPLAB X IDE I get the following error message " Cannot find Java 1.7 or higher"
Besides, I can't unintall MPLAB.. when I run the unisntaller I get an error message and application exits.
Please help.
Thanks in advance.
#1

2 Replies Related Threads

    KTrenholm
    Super Member
    • Total Posts : 788
    • Reward points : 0
    • Joined: 2012/08/08 14:04:23
    • Location: Connecticut, USA
    • Status: online
    Re: MPLAB X 5.65 doesn't find JAVA 2019/04/11 08:34:14 (permalink)
    +1 (1)
    I assume you mean 5.15, since that's the latest version.
    MPLAB X installs it's own instance of JRE, separate from the one installed previously, so it sounds like it's probably an installation problem.
     
    What error do you get when you attempt to uninstall?
    Have you tried re-installing over your current install?
     
    Have you tried this?
    https://www.microchip.com/forums/m797460.aspx
    post edited by KTrenholm - 2019/04/11 08:49:32
    #2
    Javier Lopez
    Pulsotron designer
    • Total Posts : 67
    • Reward points : 0
    • Joined: 2019/02/27 09:59:32
    • Location: Spain
    • Status: offline
    Re: MPLAB X 5.65 doesn't find JAVA 2020/05/26 05:27:52 (permalink)
    0
    I had the problem with 5.4 and solved installing both: MPLABX IDE and also the IPE
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5