• AVR Freaks

Hot!Harmony V3 package download problem

Author
Johnny0099
Super Member
  • Total Posts : 156
  • Reward points : 0
  • Joined: 2015/06/20 00:33:20
  • Location: 0
  • Status: offline
2019/04/10 08:06:15 (permalink)
0

Harmony V3 package download problem

During the package download within MPLAB 5.15, the procedure stops (hangs), see attached screen.
Any workoround?

Attached Image(s)

#1

3 Replies Related Threads

    JPortici
    Super Member
    • Total Posts : 668
    • Reward points : 0
    • Joined: 2012/11/17 06:27:45
    • Location: Grappaland
    • Status: offline
    Re: Harmony V3 package download problem 2019/04/10 09:11:06 (permalink)
    0
    1)Have a good connection... at times my POS internet provider decides i'm using too much bandwidth and will severly limit it until i power cycle the router (then i get a new IP) and it seemed it was stuck.
    2)Click Next and Wait. In the meantime open a support ticket asking to improve the downloader. At the moment it's very very crude and i don't know what exactly is checking, but between you click next and the moment the next window appear is making sure that the whole packages is up to date, or something.. And since there's probably a lot of blocking code the whole IDE will appear to be stuck
     
    I hope a new downloader will come with the next round of updates. (when? i don't know)
    #2
    Tim Cruise
    Junior Member
    • Total Posts : 91
    • Reward points : 0
    • Status: offline
    Re: Harmony V3 package download problem 2019/04/10 10:22:14 (permalink)
    0
    Let me remind you.  It is a very big download!  It is as big as many GB after extraction!  LoL: LoL
    #3
    JPortici
    Super Member
    • Total Posts : 668
    • Reward points : 0
    • Joined: 2012/11/17 06:27:45
    • Location: Grappaland
    • Status: offline
    Re: Harmony V3 package download problem 2019/04/10 10:51:24 (permalink)
    0
    holy.. i didn't notice. 6.65 GB Here
    #4
    Jump to:
    © 2019 APG vNext Commercial Version 4.5