• AVR Freaks

Hot!Why do I need CMSIS license when installing Harmony 3?

Author
RodoPIC
Senior Member
  • Total Posts : 173
  • Reward points : 0
  • Status: offline
2019/04/05 11:44:18 (permalink)
0

Why do I need CMSIS license when installing Harmony 3?

Hi all,
I was installing Harmony 3 and I got to the screen that shows that I have to agree with the these 3 licenses:
 
1. CMSIS License
2. MPLAB Harmony license
3. Microchip device family pack license
 
I can understand numbers 2 and 3. From what i google it looks like CMSIS is related to ARM cores. Is that it? and If I'm not using SAM devices why do I need it?
 
Thanks
#1

1 Reply Related Threads

    Nikolay_Po
    Super Member
    • Total Posts : 1858
    • Reward points : 0
    • Joined: 2012/04/01 13:49:27
    • Location: Russia, Novorossiysk
    • Status: offline
    Re: Why do I need CMSIS license when installing Harmony 3? 2019/04/08 00:52:34 (permalink)
    0
    With an adoption of Atmel, the Microchip is producing the microcontrollers with ARM cores.
    #2
    Jump to:
    © 2019 APG vNext Commercial Version 4.5