• AVR Freaks

Hot!Schmitt Trigger Inputs RD0 and RD1 Pic 18F45k22

Author
DMcAllister
New Member
  • Total Posts : 22
  • Reward points : 0
  • Joined: 2012/02/15 16:03:39
  • Location: 0
  • Status: offline
2019/04/05 10:53:01 (permalink)
0

Schmitt Trigger Inputs RD0 and RD1 Pic 18F45k22

From the Microchip spec sheet section 27.8, a Schmitt trigger buffer has a max input low voltage = 0.2 VDD and a min input high voltage = 0.8 VDD.  For VDD = 5V those values are 1V and 4V.  Yet, for my circuit, the transition from high to low is happening somewhere between 1 and 4 Volts, not <= 1V as expected.
 
ANSELD = 0 and TRISD = 1 for the ports.  Are there other configuration bits I need to set?  What else could be wrong?
 
Thanks in Advance.
post edited by DMcAllister - 2019/04/05 12:33:20
#1

3 Replies Related Threads

    Jerry Messina
    Super Member
    • Total Posts : 372
    • Reward points : 0
    • Joined: 2003/11/07 12:35:12
    • Status: offline
    Re: Schmitt Trigger Inputs RD0 and RD1 Pic 18F45k22 2019/04/05 12:43:49 (permalink)
    0
    There's nothing wrong. Those numbers are the spec limits.
     
    If you take a look at the typ Schmitt trigger graphs in figures 28-81 and 28-83 (pages 494-495) you'll see why you're seeing what you are.
     
     
    #2
    acharnley
    Super Member
    • Total Posts : 268
    • Reward points : 0
    • Joined: 2016/05/01 06:51:28
    • Location: 0
    • Status: offline
    Re: Schmitt Trigger Inputs RD0 and RD1 Pic 18F45k22 2019/04/05 15:46:09 (permalink)
    0
    If you need lower, as I did, use the DAC to set something like 0.12v, pipe this to one of the chips comparators and have your signal to the comparators negative pin.
    #3
    qhb
    Superb Member
    • Total Posts : 9919
    • Reward points : 0
    • Joined: 2016/06/05 14:55:32
    • Location: One step ahead...
    • Status: online
    Re: Schmitt Trigger Inputs RD0 and RD1 Pic 18F45k22 2019/04/05 16:43:15 (permalink)
    0
    dmcallister
    From the Microchip spec sheet section 27.8, a Schmitt trigger buffer has a max input low voltage = 0.2 VDD

    That means anything below 0.2 VDD is guaranteed to be treated as a low.
     

    and a min input high voltage = 0.8 VDD.  For VDD = 5V

    That means anything higher than 0.8 VDD is guaranteed to be treated as a high.
     
    Anything in between 0.2 VDD and 0.8VDD is in the "transition region" and might be a high or a low.
    That is how digital inputs are always defined.
     
    for my circuit, the transition from high to low is happening somewhere between 1 and 4 Volts, not <= 1V as expected.

    That is precisely as expected.
    If you expected it to switch from low to high at 1V, what did you expect to happen at 4V?
     
    Yes, a Schmitt trigger has a small amount of hysteresis (internal positive feed back), so the rising transition is at a slightly higher voltage than the falling transition to avoid oscillation at the transition point, but that's not the two limits we are talking about here.
     
     
    post edited by qhb - 2019/04/05 16:46:02
    #4
    Jump to:
    © 2019 APG vNext Commercial Version 4.5