• AVR Freaks

Hot!ECAN transmit problem on the PIC18LF46K80

Author
sstewart
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2019/03/28 08:21:12
  • Location: 0
  • Status: offline
2019/03/28 17:15:20 (permalink)
0

ECAN transmit problem on the PIC18LF46K80

Hi,
I'm having issues getting the ECAN to transmit properly from the PIC18LF46k80. The default program made by MCC sends a signal where the serial signal is spread apart on the oscilloscope (see attached photo). There seems to be extra space between signals in the same message. I can, however, correctly read in a CAN signal and process it. I have attached my code and an oscilloscope screenshot of the tx pin of my ecan output. Does anyone know what's causing this? or what steps is should take to remedy it?
Thanks,
sstewart

Attached Image(s)

#1

1 Reply Related Threads

    tam07
    New Member
    • Total Posts : 29
    • Reward points : 0
    • Joined: 2016/04/04 18:39:11
    • Location: 0
    • Status: offline
    Re: ECAN transmit problem on the PIC18LF46K80 2019/06/26 01:28:33 (permalink)
    0
    In MCC, try enabling "Software PLL Enabled" instead of "PLL Enabled".
    #2
    Jump to:
    © 2019 APG vNext Commercial Version 4.5