• AVR Freaks

Harmony Project without BSP:

Author
karan123
Super Member
  • Total Posts : 937
  • Reward points : 0
  • Joined: 2009/02/02 11:11:21
  • Location: 0
  • Status: offline
2019/03/28 09:29:38 (permalink)
0

Harmony Project without BSP:

Hello,
 
I have built hardware of PIC32MZ2048EFM144 144-Pin. Create New Project and also Use existing Demos For LCC ,Timer , USB, SDcard, ADC, UART etc with BSP .All working Fine.
 
1) How can I Create New Project and also Use Existing Demo without BSP for  PIC32MZ2048EFM100 100-Pin.
2) How can I Use PIC32MZ Existing Demos  with or without BSP for PIC32MK 100-Pin in which MHC configuration are Not available for PIC32MK Series MCU.
 
I am using Harmony V2_06.
 
--
Karan
 
 
#1

4 Replies Related Threads

    LostInSpace
    Super Member
    • Total Posts : 306
    • Reward points : 0
    • Joined: 2016/03/11 22:47:59
    • Location: 0
    • Status: offline
    Re: Harmony Project without BSP: 2019/03/28 17:02:11 (permalink)
    0
    This is what I have done in the past (it is brute force, but it works for me),
     
    * Start a new project based on the Chip that you are using
    * Either copy the Harmony settings or export them / import them to the new project.
    * Copy the source files you want and add them to the project
     
    You should have a new project with just the configuration you need without any hint of BSP.
     
    HTH
    #2
    nigelwright7557
    Super Member
    • Total Posts : 427
    • Reward points : 0
    • Joined: 2006/11/06 08:15:51
    • Location: 0
    • Status: online
    Re: Harmony Project without BSP: 2019/03/28 17:08:39 (permalink)
    0
    I just started a brand new Harmony project with the right processor.
    Then set up Harmony by hand.
    In my case it was just USB and A2D so easy enough.
     
     
    #3
    Paul PortSol
    Super Member
    • Total Posts : 611
    • Reward points : 0
    • Joined: 2015/07/03 11:52:03
    • Location: Newfoundland, Canada
    • Status: offline
    Re: Harmony Project without BSP: 2019/03/29 04:07:51 (permalink)
    0
    From a previous post...
    MHC_CreatingProjectWithoutBSP_v00PR.txt
    Paul
     
    #4
    RodoPIC
    Super Member
    • Total Posts : 187
    • Reward points : 0
    • Status: offline
    Re: Harmony Project without BSP: 2019/03/29 11:29:22 (permalink)
    0
    Just to mention here to remember that some of the #includes <fileToInclude> may need to be manually added.
    #5
    Jump to:
    © 2020 APG vNext Commercial Version 4.5