Hot!External 20MHz not working on PIC18F4550

Page: < 123 Showing page 3 of 3
Author
jack@kksound
code tags!
  • Total Posts : 3178
  • Reward points : 0
  • Joined: 2014/05/14 10:03:19
  • Location: 0
  • Status: offline
Re: External 20MHz not working 2019/03/25 08:21:36 (permalink)
0
Gort2015
"No what?"
Agreeing with, "Hopefully NOT 3.3 volts on an 18F4550......minimum is 4.2."


Ah thanks for that I was a little slow on picking up your meaning! As there are no other comments from the OP on the supply voltage I guess we can assume no attempt to operate from 3.3 volts with that pic is in this project.
#41
Page: < 123 Showing page 3 of 3
Jump to:
© 2019 APG vNext Commercial Version 4.5