• AVR Freaks

Assembly Code to Read Humidity Sensor

Page: << < ..67 Showing page 7 of 7
Author
delfindelfin
Super Member
  • Total Posts : 387
  • Reward points : 0
  • Joined: 2017/01/19 12:32:58
  • Location: Mexico
  • Status: offline
Re: Assembly Code to Read Humidity Sensor 2019/04/05 15:57:45 (permalink)
0
Well, that's just in the simulation. Probably I should check it in real life. It is strange in the digital analyzer, it seems that it detects when RC2 is low, and it seems that the LCD is working correctly, but the LCD simply doesn't turn on

MPLAB X IDE v5.05
XC8 2.00
Page: << < ..67 Showing page 7 of 7
Jump to:
© 2020 APG vNext Commercial Version 4.5