• AVR Freaks

Hot!Advisory 2051 License issue when PRO licensed

Author
jtnum
Starting Member
  • Total Posts : 44
  • Reward points : 0
  • Joined: 2003/11/07 12:37:02
  • Status: offline
2019/03/06 10:14:20 (permalink)
0

Advisory 2051 License issue when PRO licensed

advisory: (2051) The current license does not permit the selected optimization level, using optimization level 2
Using -Os
I have a PRO License
License Status
Microchip XC License Manager Version: 2.22
License Path: C:\ProgramData\Microchip\xclm/license/\
Product: xc8 Type: Workstation Version: 1.0 Mode: PRO Key: XXXX-XXXX-XXXX-7369
(1st 12 characters changed to X)
Product: rlm_roam Type: Workstation Version: 1.0 Mode: ?
 
Is there something I need to do with the license manager?
#1

3 Replies Related Threads

    aschen0866
    Super Member
    • Total Posts : 4587
    • Reward points : 0
    • Joined: 2006/01/08 22:18:32
    • Location: San Diego
    • Status: offline
    Re: Advisory 2051 License issue when PRO licensed 2019/03/06 11:07:05 (permalink)
    +3 (3)
    If you type "xclm -licinfo xc8", what do you see in the "HPA=xyz" field? If the HPA is expired, you can't run this version of the XC8 compiler in the PRO mode because it was installed after the expiration. Your older versions of XC8, installed prior to the expiration, should still work with the PRO mode.
    #2
    arev
    New Member
    • Total Posts : 18
    • Reward points : 0
    • Joined: 2011/01/28 04:17:36
    • Location: 0
    • Status: offline
    Re: Advisory 2051 License issue when PRO licensed 2020/09/25 01:30:56 (permalink)
    0
    aschen0866
    If you type "xclm -licinfo xc8"... 

    WHERE? xclm.exe has no such parameters...
    #3
    NKurzman
    A Guy on the Net
    • Total Posts : 18975
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: Advisory 2051 License issue when PRO licensed 2020/09/25 08:29:57 (permalink)
    +2 (2)
    I would assume in a command window with the path set to where xclm is
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5