• AVR Freaks

Hot!Short-range problem with SAMR34

Author
bkcc
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2019/03/04 10:20:40
  • Location: 0
  • Status: offline
2019/03/04 17:12:55 (permalink)
0

Short-range problem with SAMR34

Try the transmission between an ATSAMR34-XPRO kit to a Kerlink gateway model WIRNET iFEMTOcELL and at a short distance it works very well. The problem is that I can not transmit more than 150/200 meters, the antenna of the gateway is the one that brings the equipment (original) and the kit is an antenna well adapted to the band of 915Mkh (which is what I use). Can someone help me with this dilemma?
#1

1 Reply Related Threads

    mrpackethead
    packet mangler
    • Total Posts : 967
    • Reward points : 0
    • Joined: 2007/04/01 23:33:39
    • Location: 0
    • Status: offline
    Re: Short-range problem with SAMR34 2019/04/19 17:08:08 (permalink)
    0
    The supplied antenna with the ATSAMR34-XPRO is not so good. Its has quite a poor VSWR, ( > 3 ) AT 915mHZ.     Having said that i've achieved distances of greater than 6km with it.  My gateway was a RAK831 with a 9dbi dipole.
    #2
    Jump to:
    © 2019 APG vNext Commercial Version 4.5