TCP/IP Lite stack ( can use ports)

Author
harivtech
New Member
  • Total Posts : 7
  • Reward points : 0
  • Joined: 2017/07/07 12:16:20
  • Location: 0
  • Status: offline
2019/02/28 12:00:51 (permalink)
0

TCP/IP Lite stack ( can use ports)

Hi All,
Today i facing a unique problem, I am developing a tcp/ip client solution using
ENC28j60 and mcu is pic18f26k40
and mplab 4.15 and xc8 version 1.42
 
also i have a vb.net server code , I have successfully connected to server code and can transact data ,
every this fine until i access to any of the system resource like SPI2, or PORTB or PORTA
the tcp ip stop responding to the server so the stack goes timeout and try to connect again and again but never happens.
 
in any form there is problem i tried access through timer0 or i tried in the main while loop with flag set on tcp ip data arrival
but still the problem continues. i have attached the source file,
 
Any clues will be gratefull
 
with regards
 
Hari Haran.C
 
 
 
#1

0 Replies Related Threads

    Jump to:
    © 2019 APG vNext Commercial Version 4.5